MC13224 low power mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13224 low power mode

1,378 Views
andreato
Contributor I

Hallo,

I need to put the MC13224 in low power mode. The problem is that this node is a coordinator that works as a remote and portable controller. The beekit permits the low power mode only for an end device. In my case I have a network where the coordinator asks and the others answer so I can decide when weak-up. Can some one give me info about how to configure or change the beekit generation tu put a coordinator in low power?

Thank you.

Regards

0 Kudos
2 Replies

365 Views
giada
Contributor I

hello,

i'm testing low power mode on mc13224v, in hibernate mode i use 2KHz internal oscillator. This can change from 1KHz to 4KHz, but i see a frequence of 20KHz! It's too differente!

Only changing Ftune and Ctune of RING_OSCILLATOR_REGISTER i have 2KHz.

Can someone help me?

 

bye

Giada

0 Kudos

365 Views
redbee
Contributor III

Giada,

 

When I use the "2kHz" internal oscillator I first run the calibration sequence using CAL_CNTL to determine exactly was speed it is running at. I then use this calibrated clock to determine how many cycles to sleep for.

 

You can find an example of this here:

 

http://git.devl.org/?p=malvira/contiki-mc1322x.git;a=blob;f=cpu/mc1322x/crm.c

 

at the bottom.

 

-Mar.

0 Kudos