upload uClinux on MCF5329

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

upload uClinux on MCF5329

Jump to solution
1,276 Views
DarioD
Contributor I

Hi!

    Where can I find a guide for install/use uClinux on my MCF5329?

    Can I manage its GPIOs easily? And how?

Thanks and best regards,

Labels (1)
0 Kudos
1 Solution
424 Views
obidon
Contributor III

You can install following the instructions included with the board support package. http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061033202A9 If you are using Fedora 9 it installs with no problems. For Fedora 10 or 11 you may get an error about rpm-build. There is another thread relating to that. Since the 5329 is a non-MMU micro and there is no problem accessisng GPIOs. You can write or read them directly just like with a non-OS application.

View solution in original post

0 Kudos
1 Reply
425 Views
obidon
Contributor III

You can install following the instructions included with the board support package. http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061033202A9 If you are using Fedora 9 it installs with no problems. For Fedora 10 or 11 you may get an error about rpm-build. There is another thread relating to that. Since the 5329 is a non-MMU micro and there is no problem accessisng GPIOs. You can write or read them directly just like with a non-OS application.

0 Kudos