I have two sets of MC9SDT256B based systems. oscillator freq. 4.0Mz. so bus frequency should be 2.0Mz with PLL clock "disabled". After I build up a project with codewarrior. Codewarrior waywardly
sets the internal bus clock 8.0Hz. If I set up my timers literally according to the real value. i.e. I need
PWM frequency 45Hz. I setup PMW frequency in codewarrior 45Hz.I would get 11.0+Hz. Also, my pulse
width measurement also shows the reading pulse width is 4 times as the real ones. This seems not quite right although I can justify manually. Please check the attached screen shot of the setup.
What mistakes could I make?
Any response would be really appreciated
Hello,
Could you please verify that value in "Clock frequency [MHz]" property in the CPU bean corresponds to the value of the oscillator on your board?
Please find attached screen shot of CPU bean setting.
best regards
Vojtech Filip
Processor Expert Support Team