AnsweredAssumed Answered

ZStar3 Demo with VS2008 .net 3.5

Question asked by xxx xx on Jul 2, 2009
Latest reply on Jul 7, 2009 by Petr Gargulak

Hi

 

I've a question concerning the Demo applikation "ZSTARLIB_EXAMPLE". I can successfully compile and run the app. , but i get no data from my sensors. It seems that no event callback is triggert?

I've not changed anything in the demo source.

The  zstarlib.dll is included.

I can see that the com. port is successful opened and i can query the rssi for the first sensor, but i do not get burstdata? or any other event from the API.

 

Are ther any newer Version of the demo app available?

Are there any special commands/methods which have to be called to get the sensors working?

If i run the "Zstar_Demo" app. i can see the sensor data, and everything works well?

 

I'm using VS 2008 SR1 with .net 3.5 SR1

 

thx for your help

 

Mario

Outcomes