I would like to connect to my board using just a word and not an IP.
I've been looking for these network parameters but still don't exactly know what to do with them:
LWDNS_server_ipaddr
IPCFG_default_ip_address
IPCFG_default_ip_mask
IPCFG_default_ip_gateway
Is it possible to do this with the firmware and stack provided?
If anyone has an idea or comment about this, feel free to post it.
Regards,
Hello,
You probably need a DNS resolver to connect the board with domain name instead of IP address.
You can find informations about DNS resolver in MQXRTCSUG.pdf chapter 5.4.
Emmanuel
Thank you, I believe the information I was looking for is in that user guide. I did change the variables suggested in the guide, but unfortunatelly, I couldn't call the function DNSinit() because I didnt know which file to include. Since I dont know if this function is called in MQX libraries I typed different things in the address bar from the browser(ns.arc.com for instance) to check if it worked but it didnt...
I will deeper check the guide in order to make this work.
Regards