dipinraj damodaran

MCF51JM128, LQFP 64 Package and OTG Confusion

Discussion created by dipinraj damodaran on Jun 29, 2009
Latest reply on Dec 3, 2009 by dipinraj damodaran

i intend to implement On-The-Go capability into my USB gateway device which works on Freescale's MCF51JM128.

I am having a little confusion as the LQFP 64 pin package which i'll be using is lacking USB_ID Pin(pin#40 pin of LQFP80).Henceforth, how should i proceed in realizing OTG in my device?

Also, i am using the CMX stack, what changes do i need to bring about in the stack? Will it work if i configure any other GPIO pin as USB_ID pin or should i?

please help !

Thanks 
DIPIN

Outcomes