AnsweredAssumed Answered

USBDM_JM60 TBDML errror message

Question asked by Raghavendra Harikantra on Jun 22, 2009
Latest reply on Aug 11, 2009 by pgo

Hello everyone,

                      i have rigged up the ckt for BDM pod given in USBDM_JM60 distribution, and have tried the download code for hcs12 target (mc9s12dg256) using TBDML. it works well till the selection of the target(we have to manually select the target as TBDML does not identify chip id(0x0033), and the progress bar moves upto 33% and after that i get an error message saying"Error while loading diagnostics alogrithm to Target system.The chip may be secured ,or the derivative selected may be wrong".

 

So if anyone knows solution to this plaese reply.  

     

Outcomes