Sathish Kumar P S

Fast code download to target(MPC8569E)

Discussion created by Sathish Kumar P S on Jun 13, 2009
Latest reply on Jun 17, 2009 by Ronald Collins
I have not checked "Do not use fast download" in my Connection Settings.
During by debugging in IDE, code is downloaded at faster rate.
 
But when I download the code to target using CCS, download speed is less(it does not use fast download).
 
DriverVer=08/20/2007, 9.0.0 
  
Commands used to run download and run the elf
 
setads 8569ads 1
reset
ccs::set_max_tck 0 12000
load TEST_RUN.elf
args 0x80 1770405119
clear
go 

Outcomes