I'm trying to running ltib but it stops when it tries to reach wwwgate0.freescale.net
I've tried to ping this ip from 3 different connection with 3 different dns and no one returns an answer.
How could bypass this problem?
Thanks
Solved! Go to Solution.
This is a freescale internal proxy. If you are not inside of the freescale internal web,
you should/can not use it. The description sounds like you run a fsl internal setup from outside.
If you are direcly connected to the internet, just remove the proxy configuration.
Daniel
This is a freescale internal proxy. If you are not inside of the freescale internal web,
you should/can not use it. The description sounds like you run a fsl internal setup from outside.
If you are direcly connected to the internet, just remove the proxy configuration.
Daniel