Hi
I have a coordinator node (MC1322x Sensor Node) and have another node (my board) with MC13224V rev 2.1
The codebase in both are correct.
In the coordinator node i have 22 endpoints and in my board i have 16 endpoints. Well, i can bind key between boards and works fine. In both i receive BindSuccess and the led stop flashing.
But when i try to send a ASL_ZclOnOffReq from by board to coordinator board i can't. I receive the zbStatus_t with the value 0xA4 that can meaning gApsInvalidBinding_c or gZbInvalidEndpoint_c. The second value is not possible because the value of endpoint is correct (between 0x01 and 0xF0).
What I am doing wrong? Any suggestion would be appreciate....
Thanks
Added p/n to subject.
Solved! Go to Solution.
Sorry everybody
I could see my error
My application (in both boards) can't register more than 4 endPoints...
Now, i need to understand why...
Regards
Sorry everybody
I could see my error
My application (in both boards) can't register more than 4 endPoints...
Now, i need to understand why...
Regards