Hello every body
nice to met us
Some one can help me i cant install codewarrior for microcontrollers V62 In Windows vista 64 bits the installer has no errors but cant complete the installer
Solved! Go to Solution.
I am sorry, but that version of CodeWarrior software only works with 32-bit Microsoft Vista.
---Tom
I installed the application under Vista 32-bit on a separate partition, then in x64 Windows-7, ran D:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\bin\regservers.bat first and the program has worked just fine. I haven't tried copying the folder across and am still running from the D drive. This shows that the problem is primarily with the installer and not CodeWarrior!
I am sorry, but that version of CodeWarrior software only works with 32-bit Microsoft Vista.
---Tom
Thanks Tom, so what can i do, i dont have other computer and the OS is original. there is no way to install the program?