S32K148 reset Led

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 reset Led

1,094 Views
faress_mansouri
Contributor II

Hello,

when i try to download my code in s32k148 card, i get this error :

pastedImage_2.png

and :

   - the reset LED is turned ON 

   - the MCU is heating.

pastedImage_1.png

does that means that my card is damaged ? if not what can i do to fix this problem ?

Thanks,

Tags (1)
2 Replies

1,024 Views
Jeremy_He
NXP Employee
NXP Employee

I have met a few times that VDD and GND are shorted somehow.  You may check that using a multimeter. If that happens, the MCU is mostly damaged. 

1,024 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Faress,

Unfortunately, due to the reset pin is being forced to a low state and the MCU is heating is very likely it stops working. 

Best Regards,

Alexis Andalon