S32 Design studio shows no license after installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design studio shows no license after installation

4,001 Views
jainsubhav
Contributor I

After installing S32 DS, I am getting following message 

S32 Design Studio for ARM

 

no FNP_Act_Installer in java.library.path

Also there are no log files generated.

Tags (2)
0 Kudos
11 Replies

2,815 Views
whinojo
Contributor II

Seen same error. Is there any solutions for this? Regards.

0 Kudos

2,811 Views
mikedoidge
NXP Employee
NXP Employee

Hello @whinojo,

S32 Design Studio is developed for and tested to work on Windows and Linux. For Linux, the Ubuntu, Debian, and CentOS are options. To see which versions are supported, please check the release notes document. We cannot guarantee it will work on any OS not listed in the release notes. You are on your own for any issues encountered if you choose to install to anything which is not listed.

Best Regards,

Mike

0 Kudos

2,801 Views
whinojo
Contributor II

Hi, I have the software installed in Windows.

Regards.

0 Kudos

2,797 Views
mikedoidge
NXP Employee
NXP Employee

Hello @whinojo,

Please provide the logs:

C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs

"C:\Users\{userid}\workspaceS32DS.ARM.2.2\.metadata\.log"

Best Regards,

Mike

0 Kudos

2,783 Views
whinojo
Contributor II

Thanks for the quick reply. Please find attached the requested logs.

Best regards.

0 Kudos

2,778 Views
mikedoidge
NXP Employee
NXP Employee

Hi @whinojo,

I checked both log files - thank you for providing them.

It seems something happened to the license after installation and activation. Let's try to solve this by the following method:

Trusted Storage is corrupted and needs to be re-initialized.

Windows host:

-> Delete 'C:\ProgramData\FLEXNet'

This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.

After this, you should be able to re-activate the existing license on your PC

Best Regards,

Mike

2,759 Views
whinojo
Contributor II

Good afternoon Mike, I did the recommended deletion of the directory, re-started DS and I got the message in the attached image. The message seem to have the "Activate" button disable. Pressing close just closes the S32 DS application completely. Please advise.

Best regards.

William

0 Kudos

2,755 Views
mikedoidge
NXP Employee
NXP Employee

Hello @whinojo,

Please check your S32 Design Studio installation. Specifically check the following file:

s32ds.ini

image.png

You need to check it for this line:

image.png

If this line is missing or set to the wrong path, then it will produce the error you reported.

If the FNP_Act_Installer.dll file is missing from the ...cll/i86 (or x64) folder, or any of these things are not right, it might make sense to install again. Though the installation log looks good, it's possible something did not install correctly and could be resolved via reinstall.

Please let me know your findings.

Best Regards,

Mike

0 Kudos

3,566 Views
driftregion
Contributor I

Installing on wine, I found the same error `no FNP_Act_Installer in java.library.path`

when executing

`C:/NXP/S32DS_ARM_v2.2/eclipse/s32ds.exe`

 

However,

`C:/NXP/S32DS_ARM_v2.2/eclipse/eclipsec.exe`

launched without error.

0 Kudos

3,628 Views
johnkevintoral
Contributor II

Hi, has anyone solved this yet? TIA

0 Kudos

3,835 Views
Samuel_2015
Contributor I

I also encounter this problem, have you solved it??

0 Kudos