HI
i'm using i.mx6Ul and i'm tring to change resolution size from 480x272 to 240x156 by using xranr command
i used command following way
$xrandr --newmode "240x135_60.00" 2.25 240 248 264 288 135 138 143 146 -hsync +vsync
$xrandr --addmode XWAYLAND0 240x135_60.00
$xrand --output XWAYLAND0 --mode 240x135_60.00
then i got following error
#################################################################
X Error of failed request: BadValue (integer parameter out of range for operation)
Major opcode of failed request: 139 (RANDR).
Minor opcode of failed request: 7 (RRAddOutputMode).
Value in failed request:0x0 Serial number of failed request: 22.
Current serial number in output stream: 23
#################################################################
i want now how to solve this error.
or any otherway to change resolution size
Which version BSP are you using? You need to confirm if these resolutions are supported first and then you can use.
how can i check that?
is that same version as linux-yocto kernel?
When your board system boot up, you can go to /sys/class/graphics/fb0, use the cat modes to list all the mode. You can try this.
sorry for late respond
i found that my bsp is not supported
thanks for help