Hi, eveyone!
I am now developing one mcf52211 board. and buy one TBLCF BDM pod. and using cw 7.1 special edtion. But when I click"debug" button, I always get:"could not open memory configuration file"; I don't know how to set the memoery configuration file in CW. any suggestions?
thanks in advance!
Solved! Go to Solution.
First, did you use the CodeWarrior Project wizard to set up your project, or start it from scratch (Empty Project)? If you use the wizard, it normally sets up the configuration file for you. You can select the memory configuration file to use from the project settings panel. Type Alt+F7 to bring up the project's settings panel. Select the CF Debugger Settings panel. On this panel you'll see the option for Use Memory Configuration File. You can use the Browse button to choose a different memory configuration file, one that better matches your target board.
---Tom
First, did you use the CodeWarrior Project wizard to set up your project, or start it from scratch (Empty Project)? If you use the wizard, it normally sets up the configuration file for you. You can select the memory configuration file to use from the project settings panel. Type Alt+F7 to bring up the project's settings panel. Select the CF Debugger Settings panel. On this panel you'll see the option for Use Memory Configuration File. You can use the Browse button to choose a different memory configuration file, one that better matches your target board.
---Tom