No source available for "0x410"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No source available for "0x410"

1,715 Views
oceansea
Contributor III

hi,i use the S32DS for ARM 2018.R1  develop  S32K146 MCU;

Yesterday, the project is  ok ,i can debug my software.

Because yesterday i backup and delete it,  today i import  this prj to S32DS, and i want debug ,but it show this

No source available for "0x410"   and it can't  step by step.

Then ,i try to clean the and rebuild the prj ,it still can't debug.

I  check  all the file path , not any problem

pastedImage_1.png

Labels (1)
0 Kudos
1 Reply

1,662 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Ocean,

Are you using the same debug session created for the previous project or did you create a new one? This memory section corresponds to the reset handler so I think something is wrong with the path.

Also, be sure that the path file in the debug session is the same as your project.

Best Regards,

Alexis Andalon

0 Kudos