AnsweredAssumed Answered

bitbake imx-image-multimedia error:assimp_5.0.1.bb:do_compile

Question asked by jingjie he on Jul 31, 2020
Latest reply on Aug 5, 2020 by jingjie he

when i try to compile imx8qxp's image using command "bitbake imx-image-multimedia",an error occurs,here is the log:   

 

ERROR: Task (/home/he029/bin/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-graphics/vulkan/assimp_5.0.1.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2650 tasks of which 2649 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/he029/bin/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-graphics/vulkan/assimp_5.0.1.bb:do_compile
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

 

my download version is "repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.3-2.0.0.xml " ,and bitbake config"DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source imx-setup-release.sh -b build-wayland"

is it because I select  a wrong download version or wrong bitbake config?

Outcomes