Are there demo/eval boards available for MP3H6115AC6T1 or MPXAZ6115AC6T1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there demo/eval boards available for MP3H6115AC6T1 or MPXAZ6115AC6T1?

1,091 Views
ctasker01
Contributor I


Are there demo/eval boards available for MP3H6115AC6T1 or MPXAZ6115AC6T1?

Labels (2)
Tags (1)
0 Kudos
1 Reply

1,043 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, there is no evaluation board for these pressure sensors, but these are really easy to use as you can see in Figure 4 of both devices datasheets, you only need a 5V (for the MPXAZ6115AC6T1) or 3V (for the MP3H6115AC6T1) power supply connected to pin 2 (with a 100nF decoupling capacitor), connect pin 3 to GND, and connect a 47pF capacitor and a 51k resistor on the output pin (Pin 4).

The output is given right away without the need of any kind of programming or initialization.

 

There are some recommendation about how to use this kind of sensors using different mcus, for example, you can find an example using an Arduino uno board with a MPXV7025DP in the following link: http://fabacademy.org/2019/labs/bahrain/students/zahra-almukhariq/assignments/week11/#sensor-connect...

Jose

NXP Semiconductors

0 Kudos