As LSDK for layerscape processor is very large body of software , NXP should include have some training on flow of code as it is very difficult to understand the flow for beginners like me. LSDKUG is not very helpful as it only explains at top level.It does not explain on how to modify the device tree to suit our custom board and so on. Kindly help.
Use the following command sequence for LSDK2004 installing:
Install Ubuntu 18.04.
Install all updates for this Ubuntu.
Install and build LSDK2004 using the following command sequence:
Change .dts file and using the following commands for building:
flex-builder -c linux -a arm64
flex-builder -i mkfw -m ls1012afrwy -b qspi
See the AN5125 about Device Tree:
https://www.nxp.com/docs/en/application-note/AN5125.pdf
There is also information in internet about Device Tree:
https://elinux.org/Device_Tree_Reference
https://www.kernel.org/doc/Documentation/devicetree/usage-model.txt
https://www.devicetree.org/specifications/
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------