AnsweredAssumed Answered

Unable to boot openwrt

Question asked by zhangjian zhang on Jul 27, 2020
Latest reply on Jul 29, 2020 by Yiping Wang

The openwrt system of ls1043a motherboard cannot be started,  the tips are as follows: “FDT and ATAGS support not compiled in - hanging”.Please tell me what I need to do?

This is my email address zhangjian@it525.com

 

U-Boot 2018.03 (Dec 24 2018 - 01:06:38 +0000)

SoC: unknown (0x87920411)
Clock Configuration:
CPU0(A53):1600 MHz CPU1(A53):1600 MHz CPU2(A53):1600 MHz
CPU3(A53):1600 MHz
Bus: 400 MHz DDR: 1600 MT/s FMAN: 500 MHz
Reset Configuration Word (RCW):
00000000: 08100010 0a000000 00000000 00000000
00000010: 45580002 00004012 e0025000 c1002000
00000020: 00000000 00000000 00000000 00038800
00000030: 00000000 00001101 00000096 00000001
Model: LS1043A RDB Board
Board: LS1043ARDB, boot from vBank 0
CPLD: V2.0
PCBA: V5.0
SERDES Reference Clocks:
SD1_CLK1 = 100.00MHZ, SD1_CLK2 = 100.00MHZ
I2C: ready
DRAM: Initialzing DDR using fixed setting
Configuring DDR for 1600 MT/s data rate
3.9 GiB (DDR4, 32-bit, CL=11, ECC off)
Using SERDES1 Protocol: 17752 (0x4558)
SEC0: RNG instantiated
PPA Firmware: Version LSDK-18.09
Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0
QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1
Flash: 128 MiB
NAND: 512 MiB
MMC: FSL_SDHC: 0
Loading Environment from Flash... OK
EEPROM: Read failed.
In: serial
Out: serial
Err: serial
SCSI: PCIe0: pcie@3400000 Root Complex: no link
PCIe1: pcie@3500000 Root Complex: no link
PCIe2: pcie@3600000 disabled
Error: SCSI Controller(s) 1B4B:9170 not found
Net: Fman1: Uploading microcode version 106.4.18
FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6
Hit any key to stop autoboot: 0
starting openwrt ...
Trying load from SD ..
Device: FSL_SDHC
Manufacturer ID: 2
OEM: 544d
Name: SA08G
Bus Speed: 50000000
Mode : SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 7.2 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes

MMC read: dev # 0, block # 32768, count 81920 ... 81920 blocks read: OK
## Booting kernel from Legacy Image at a0000000 ...
Image Name: ARM64 OpenWrt Linux-4.14.180
Image Type: AArch64 Linux Kernel Image (gzip compressed)
Data Size: 5585812 Bytes = 5.3 MiB
Load Address: 80080000
Entry Point: 80080000
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
FDT and ATAGS support not compiled in - hanging
### ERROR ### Please RESET the board ###

Outcomes