AnsweredAssumed Answered

Pressure Sensor MPXHZ6130AC6U - Port Question

Question asked by Anthony Simbana on Jul 24, 2020
Latest reply on Jul 27, 2020 by Jozef Kozon

Hello,

 

Looking to move from MPXHZ6130A6U  to MPXHZ6130AC6U. Based on the review of the datasheets, it seems both are electrically equivalent with the exemption of the dimensions, such as height.

 

Questions:

1) How does the single port on MPXHZ6130AC6U affect its performance compared to that of MPXHZ6130A6U? Are these two functionally equivalent?

 

2) Is there a height clearance recommended for the single port for MPXHZ6130AC6U?

 

3) Is there a replacement recommended by MFG for MPXHZ6130A6U that has similar tolerances or tighter?

 

Thanks,

 

Anthony

Attachments

Outcomes