MIPI DSI on imx6solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI DSI on imx6solo

1,209 Views
abhay_patil
Contributor II

Hi, team,

       I am working imx6solo and I am having Linux 5.0 kernel and one MIPI display (vendor-LEADTEK)

I am having reg commands with me what I have to try to get FB and MIPI DSI  working 

I tried with 

MIPI DSI display problems 

i.MX6 MIPI-DSI Display ( ST7701 controller) 

MIPI Display interface 

I am having details of reset pin and I am providing correctly as per the hardware team instructed.

as I am seeing in kernel 5.0 there is a missing driver of framebuffer compatible = "fsl,mxc_sdc_fb"

also driver for MIPI DSI compatible = "fsl,imx6q-mipi-dsi"

please suggest any solution to work display 

0 Kudos
4 Replies

1,093 Views
abhay_patil
Contributor II

hi team 

    i want to support 2 lane Mipi display, what options/drivers/dtsi changes needs to be done  into uboot/kernel to make display work.

0 Kudos

1,093 Views
abhay_patil
Contributor II

Hi, igorpadykov

      As I am seeing in Linux kernel 5.0 there is no support for both (frame buffer & MIPI) please provide clear vision over this as this is on the higher priority list And please provide step by step guide to work the display.

0 Kudos

1,093 Views
igorpadykov
NXP Employee
NXP Employee

Hi abhay

 

for features not supported in bsps nxp has special service for adding such

support per customers request:

Commercial Support and Engineering Services | NXP 

 

Best regards
igor

0 Kudos

1,093 Views
igorpadykov
NXP Employee
NXP Employee

Hi abhay

framebuffer support for kernel 5.0 is described in

sect.6.2.2 Frame Buffer i.MX Linux Reference Manual

support for MIPI-DSI in sect.6.4.2 MIPI DSI Interface

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos