Are the following camera options feasible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are the following camera options feasible?

440 Views
andy5
Contributor I

Are the following camera options feasible? In this scheme,the sensor's data is transmitted to imx8qm through one LVDS, in which there is one LVDS clock signal and one synchronization signal to the Mipi of imx8qm_ CSI port.

pastedImage_1.png

The problem is as follows:

The four lane channels of MIPI_CSI seem to be used to receive data. Now I want to use one lane of the Mipi_CSI lanes as the sensor data receive lane and other one lane to be used as the Synchronous signal receive lane, is it feasible? 

Thank you for the answering the above question!

Tags (1)
0 Kudos
0 Replies