Emmc UUU flashing of signed ahab images to imx8qxp Evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Emmc UUU flashing of signed ahab images to imx8qxp Evk

932 Views
vimalbabu
Contributor II

We are trying to flash cst signed ahab images to imx8qxp evk. The following are the images in hand

  • container with singed uboot ----> flash.bin
  • container with signed Image and dtb ---- > Image
  • custom-base-image-imx8qxp-20200720055835.rootfs.wic.bz2 , we are using this wic image such that we will replace the uboot and Image with signed flash.bin and Image

Method used to replace uboot 

  1. Unzip the wic.bz2, we get custom-base-image-imx8qxp-20200720055835.rootfs.wic
    1. $ bzip2 -vfd custom-base-image-imx8qxp-20200720055835.rootfs.wic.bz2
  2. Replacing unsigned uboot with signed flash.bin
    1. $ sudo dd if=flash.bin of=custom-base-image-imx8qxp-20200720055835.rootfs.wic seek=33 bs=1k
  3. Using wic command we replace Image with signed Image container
    1. $ wic cp Image custom-base-image-imx8qxp-20200720055835.rootfs.wic:1
  4. Flashing wic image to evk
    1. $ sudo uuu -b emmc_all flash.bin custom-base-image-imx8qxp-20200720055835.rootfs.wic

Can you please confirm regarding this method of emmc flashing? 

0 Kudos
2 Replies

587 Views
pawar_123_y
Contributor II

Hello Joanxie,

I want to flash signed image using uuu on imx8qxp. i used sudo uuu -b emmc_all uboot rootfs.wic(this is unsigned image) command everytime. Can you please tell me which command i should used for signed image. name of signed image is now flashed.signed.bin .                              should i try with sudo uuu -b emmc_all uboot(AHAB-ENABLE) Flashed.signed.bin(this signed image include SCFW, SEFW,ATF,uboot)                                                                                  

0 Kudos

895 Views
joanxie
NXP TechSupport
NXP TechSupport

I have already mailed to you, pls refer to it

0 Kudos