AnsweredAssumed Answered

Question about host usb hid on imxrt1010 connected with PS3

Question asked by Minh-thuc PHAM on Jul 17, 2020
Latest reply on Jul 31, 2020 by Felipe García

Hi all,

When i customized the example host_hid_generic_bm on board imxrt1010, i had a problem that the function callback USB_HostHidInCallback is not returned even the failed status. But after unplugging the joystick PS3,  this function will be called for one times. I can't understand what is  the influence of the action plugging on the function callback. Someone can figure out what is the problem in this case, please?

Can i create a host usb hid for imxrt1010 for the controller PS3 or this host usb can run only with mouse, keyboard, generic? 

 

Regards

 

Thuc 

Outcomes