I'm looking for a development board for LPC11E37 but i didn't find any solutions.
I find only a LPCXpresso board for LPC11U37H for LPC11U Not E.
LPCXpresso board for LPC11U37H | NXP
What is the differences in the microprocessor. Are they compliant in registers?
Is there a board for LPC11E37??
Thanks
HI
You can use LPCXpresso board for LPC11U37H | NXP for LPC11E37. you can connect and debug LPC11E37 code on this demo board without issue.
The difference between these two parts is, LPC11U37 support full speed USB while LPC11E37 can't support USB.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------