AnsweredAssumed Answered

iMXRT1064 Coin Cell or Supercapacitor usage

Question asked by Nikhil Sawane on Jul 13, 2020
Latest reply on Jul 23, 2020 by Nikhil Sawane

Hello, 

 

I am working on a project with iMXRT1064. 

I am using a SuperCapacitor as a replacement for a coin cell battery. 

As per indications on the development kit schematic, I connected supercap to VDD_SVNS_IN.

 

However, the MCU does not start working until the capacitor has been discharged. 

So after use, I have to wait 15 to 20 minutes to get the board running again. 

 

Looking at the datasheet, i found that VDD_SVNS_IN pin is multi-featured. RTC is one of the feature.

Could it be that this pin is by default set to GPIO which could be a high drain source?

This could explain why the board does not power up till capacitor has been discharged? 

 

If yes, in order to use a coin cell or supercap, do we need to configure this pin to RTC?

 

Thank you,

Nikhil 

 

 

Outcomes