AnsweredAssumed Answered

RT1050/1060 - Where is the LCD_RESET signal?

Question asked by David Rodgers on Jul 13, 2020
Latest reply on Jul 27, 2020 by David Rodgers

I'm looking at the RT1060 reference manual, and in "Table 35-5 - Pin use in DOTCLK mode", at the end of the table, an LCD_RESET signal is mentioned.  The string "LCD_RESET" does not appear anywhere else in the document.  It is not mentioned in the datasheet.  Google reveals an app note AN12302 "i.MX RT eLCDIF RGB Mode Use Case" which mentions the LCD_RESET signal but doesn't define where it appears.  The LCD_RESET signal also does not appear anywhere in the MCU Config Tools pin selector under the LCDIF column.

 

Does the LCD_RESET signal actually exist?  Or is this an artifact from an older revision of the reference manual?

 

David R.

Outcomes