mpc5777c (mpc5775e) FEC send/receive only once

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc5777c (mpc5775e) FEC send/receive only once

659 Views
leonggz
Contributor I

hi, i have a custom board using 5777c/5775e with TJA1100 running in autonomous mode with MII-Lite configured on the mpc side. 

I was able to send and recieve packets one time upon power up but further sends would not show up on the TX lines (scope) or PC end (wireshark). the receiver is interrupt driven so it hits once then no more packet is detected.

i've disabled the D-cache as some suggested but the same results. 

the argument is that if the send/receive works one time then the hardware and phy chip should be ok. so the focus is on the driver end. 

any hint is welcome.. i'm out of ideas... 

thx

Labels (1)
0 Kudos
1 Reply

611 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

please refer to https://community.nxp.com/thread/537336 

BR, Petr

0 Kudos