Now I used 5.4.3 Linux + imx8mq board, and I would like to boot the jailhouse root cell, when I run jh_mmcboot in u-boot, it hang at rootfs with sd card as blew:
It seems the sd card issue, but I have modify any code.
Could anyone alse face this issue ?and How can fix it ?
BR
And the 4.4 kernel version is no this issue.
Hi Hongxing,
In this release, the virtualization (Xen, Jailhouse) feature is not verfied or tested. Recommend you to use other version BSP.
Have a nice day
Best Regards
Rita
Is there anyone face the same issue ?