HID(R) :LIBUSB_ERROR_TIMEOUT in IMX8QXP C0 SDPS download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HID(R) :LIBUSB_ERROR_TIMEOUT in IMX8QXP C0 SDPS download

727 Views
mashaofeng
Contributor III

dear expert :

    now our product switch to  imx8qxp c0 chip , we try to download c0 image in sdps , but  when we run :

     sdps: boot -f flash.bin

     if show error  HID(R) :LIBUSB_ERROR_TIMEOUT immediately  , we captured usb bushound log , only follow log printed when run download cmd:

   

6.0  CTL    23 03 02 00  04 00 00 00                                                                                CLASS                                   30.1.0       

   6.0  CTL    23 01 02 00  04 00 00 00                                                                                CLASS                                   31.1.0       

   7.1  IN     10                                                                                                      .                                       32.1.0       

   6.0  CTL    a3 00 00 00  04 00 04 00                                                                                CLASS                                   33.1.0       

   6.0  IN     03 05 04 00                                                                                             ....                                    33.2.0       

   6.0  CTL    23 01 12 00  04 00 00 00                                                                                CLASS                                   34.1.0       

   6.0  CTL    a3 00 00 00  04 00 04 00                                                                                CLASS                                   35.1.0       

   6.0  IN     03 05 00 00                                                                                             ....                                    35.2.0       

   6    CMD    00 00 00 00  00 00 00 00  01 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  20 d5 b4 ad  09 c6 ff ff  TEST UNIT READY                         36.1.0(2)    

                    00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00                                          36.1.32      

                   00 00 00 00  00 00 00 00  13 00 08 02  53 65 54 6c  e5 c6 0e 27  38 52 38 d7  b0 11 94 a8  09 c6 ff ff                                          36.1.64      

                   70 ec 4c af  09 c6 ff ff  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00                                          36.1.96      

                   00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00                                          36.1.128     

                   00 00 00 00  00 00 00 00  00 00 00 00  00 00 00 00  00 00 00                                                                                    36.1.160     

   6    SSTS   00                                                                                                      pending                                 36.2.0       

   6.0  CTL    23 03 02 00  04 00 00 00                                                                                CLASS                                   38.1.0   

then it show error and no other log print;

why this happened ?  what should i do ?

thanks

0 Kudos
1 Reply

694 Views
igorpadykov
NXP Employee
NXP Employee

Hi ma

one can try suggestions on

issue to flashing the i.MX 8M Quad EVK Board · Issue #72 · NXPmicro/mfgtools · GitHub 

WIN7 User Guide · NXPmicro/mfgtools Wiki · GitHub 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos