Unable to arm the Hovergames drone with the FS-i6S controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to arm the Hovergames drone with the FS-i6S controller

3,013 Views
raymond_ytsiu
Contributor I

I tried to follow the step #4 (https://nxp.gitbook.io/hovergames/userguide/flying/before-you-fly ) to arm the Hovergame drone but it failed on my step 2 below. The four motors do not spin at all.  

Can I get some help on how to troubleshoot this? 

Arm the drone, which is a two-step process involving both the drone and the RC transmitter:

  1. Arm on the drone-side by pressing and holding the safety switch on the GPS module, until it starts blinking faster.

  2. Arm on the RC transmitter-side by holding the left stick to the bottom right, until the safety switch and RGB LED on the FMU glow solid. A some help on how to troubleshoot this? t this point the drone is armed!

0 Kudos
5 Replies

2,889 Views
iaingalloway
NXP Employee
NXP Employee

Hi @comptonben 
There are a number of failsafes and steps before the drone will arm and the motors spin.
I don't think we heard a final resolution from @raymond_ytsiu , but i do think at one point he had the usb cable still connected to the FMU, and the drone will definitely not arm with that cable connected (unless very specific overrides are turned on)

Can you give more details as to what your specific situation is?

Have you:
- Calibrated all the sensors
- checked that you have RC communication working right

- Telemetry working to the drone?
- What errors are showing in QGroundControl if any? (there is a pre-flight checklist and also a warning box area.)
- do you have a GPS lock
- has the arming switch been pressed on the GPS
- is there a kill switch configured in failsafe settings that may be on?
- could you have set a GEOFENCE and maybe you are outside it?
- Do you hear the motor ESCs make their power up tune-sound.
- have you tested the motors manually with the propellers off?

Happy to help - please share a bit more detail.

2,884 Views
comptonben
Contributor I

Re-flashed the firmware and re-calibrated everything and then it armed and is functioning correctly!

 

Thanks,

Ben

0 Kudos

2,898 Views
iaingalloway
NXP Employee
NXP Employee

This question is being addressed by nxf48254 and landonh12 on the PX4.io slack channel. We will summarize here shortly.

0 Kudos

2,892 Views
comptonben
Contributor I

Was there any headway on this issue? I am running into it as well.

0 Kudos

2,800 Views
ath
Contributor I

Same here.

Have you managed to solve the issue by any change?

0 Kudos