BFU550 ESD characteristics

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BFU550 ESD characteristics

595 Views
a-kondo
Contributor I

BFU550のデータシートに記載されているHBMの値とCDMの値は正しいでしょうか。HBMが150Vというのはあまりにも弱すぎますし、CDMの値が2kVというのは非常に強いと思います。

Are the HBM and CDM values on the BFU550 data sheet correct?

It's too low for the HBM and too high for the CDM.

Labels (1)
  • RF

0 Kudos
1 Reply

547 Views
LPP
NXP Employee
NXP Employee

BFU550 ESD specs in the datasheet comply with Product Qualification report.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos