AnsweredAssumed Answered

S32G-PROCEVB-S (S32G274A) DDR Tool Failure

Question asked by Bishoy Rafaiel on Jul 3, 2020

I'm currently trying the DDR tool in the S32 Design studio using the evaluation board "S32G-PROCEVB-S" with the following extensions installed:

Package: NXP GCC for Arm Embedded Processors v9.2 build 1627; Version: 1627; Build id: 202003031402
Package: S32 Design Studio Platform Tools package; Version: 3.2.2; Build id: 202004222055
Package: S32G2xx development package; Version: 3.2.2; Build id: 202004222145
Package: S32SDK S32G274 BETA 0.9.0; Version: 0.9.0; Build id: 202003261626
Package: S32 Design Studio Platform package; Version: 3.2.2; Build id: 202004222055
Package: NXP GCC for Arm Embedded Processors Build 1574; Version: 1574; Build id: 201909041333
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 201909041409

 

The problem is that it stucks upon the execution in a state called "APP_WAIT_FOR_INPUT" where it read the value "AA55AA55" continously without ending the execution and without generating the code as well.

 

I've treid this with SDK S32SDK S32G274 BETA 0.9.0; and with S32SDK S32G274 EAR 0.8.0; as well

Also I've tried with the serial and with the S32 Debug probe and I get the same result in both

 

Attached below the debug log of the execution so I'd appreciate someone can pin-point where the problem is, Is there any switch or jumper configuration that need to be done on the evaluation board  itself or there's something wrong with the S32DS configuration.

Attachments

Outcomes