AnsweredAssumed Answered

SE050: key rotation: DoAPDUTxRx_s_Case4 returns 0x6a80

Question asked by Jorge Ramirez Ortiz on Jul 1, 2020
Latest reply on Jul 1, 2020 by Jorge Ramirez Ortiz

Hi all,

 

I am running the sample code from SE05X Rotate PlatformSCP Keys Demo on the SE050 ARD board (OEFID = 6). I am using simw-top version 2.14.

 

The APDU request from the sample code returns 0x6A80 (invalid policy?)

 

An object is only created if the attached policy is valid and, if the policy validation fails, the error code 0x6A80 is returned as response to the object creation command. AFAICS the sample code doesnt configure any policy. Is there anything else that needs to be done? anything that is missing?

 

many thanks in advance

Jorge

Outcomes