"Loading a new application will stop the exacution of the current one"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"Loading a new application will stop the exacution of the current one"

1,225 Views
sat
Contributor I
Hello,
I am working with EVB9S12XEP100 and when connected to BDM there are some warnings and errors on debug screen. I checked the pins and see that :

 
I see these warnings one ofter another:
first : "Loading a new application will stop the exacution of the current one"
and second : "Error Elf Loader
                       Error while writing to FFFE ... 101FE"
 
and last : "Failed to load
                 "C:\ ..... \P&E_Multilink_CyclonePro.abs"
 
And after all of these processor doesn't work. Why?
Labels (1)
0 Kudos
1 Reply

288 Views
CrasyCat
Specialist III

Hello

 

Did you look at this thread?
The message you are getting indicates you are trying to download code at address 10100-101FE, which is not correct.

CrasyCat

0 Kudos