AnsweredAssumed Answered

Question about T2080 Clock Speeds

Question asked by Louis Lo on Jun 29, 2020
Latest reply on Jun 29, 2020 by ufedor

As advertised on the T2080RDB brochure, it can run from 1200MHz up to 1800 MHz. 

 

Out of the box the T2080RDB is running at around 1800MHz, as displayed through the generic uboot when connected via UART.

 

Is there any way to tweak this such that the clock speed can be lowered, say to 1200MHz?

 

I heard from a colleague that there needs to be an RCW tweak. I'm not sure what that is as I'm fairly new to all this.

 

Please advise.

 

Thanks!

Outcomes