How to use the SFP+ ports at 1G?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the SFP+ ports at 1G?

835 Views
helloppc
Contributor I

As per question, I am using the T4240RDB and, for compatibility, I would like to use the SFP+ ports at 1G instead of 10G.

Following the fman specs, I added the property fsl,fman-best-effort-port in the dtb, but my switch can't establish the connection (Dell 5324): I tried with auto-negotiation enabled and disabled.

Should I change anything else? Or am I misunderstanding the specs of FMAN?

Labels (1)
Tags (3)
0 Kudos
1 Reply

762 Views
bpe
NXP Employee
NXP Employee

Line data rate has nothing to do with any FMAN Device Tree properties because it is selected in another module, SerDes.

SerDes mode used for connecting to  SFP+ interfaces is XFI, which is a single data rate protocol. It will not autonegotiate

and switch to 1G. You have to perform  a full reset with another RCW to switch the SerDes lane to SGMII/1000Base-KX.

-------------------------------------------------------------------------------

Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------


Have a great day,
Platon

0 Kudos