AnsweredAssumed Answered

LS1021ATWR Fuse Provisioning Firmware

Question asked by Elias Bitbaker on Jun 26, 2020
Latest reply on Jul 6, 2020 by bpe

I am trying to implement Secure Boot + Chain of Trust w/Confidentiality. I am following the steps outlined in Section 6.1.4: Procedure to enable Secure Boot in the LSDK User Guide Rev 19.09_311219. 

 

I have built the CST and generated keys and built the LSDK composite secure boot firmware. I am now on Step 4: Generate Fuse Provisioning Firmware. This links me to Section 6.4.4 in the user guide. In Step 3: Generate BL31 image with fuse provisioning support, it says to run the following command: 

   flex-builder -c atf -m <machine> -b <boottype>

so I run:

   flex-builder -c atf -m ls1021atwr -b sd

and I get the following output: 

root@538bbf29aa5d:/flexbuild# flex-builder -c atf -m ls1021atwr -b sd
COMPONENT: atf
MACHINE: ls1021atwr
BOOTTYPE: sd
make: Entering directory '/flexbuild'
make[1]: Entering directory '/flexbuild/packages/firmware'

Building ATF ...

Building dependent fuse_scr.bin ...

#----------------------------------------------------#
#------- -------- -------- -------#
#------- CST (Code Signing Tool) Version 2.0 -------#
#------- -------- -------- -------#
#----------------------------------------------------#

==========================================================
This tool includes software developed by OpenSSL Project
for use in the OpenSSL Toolkit (http://www.openssl.org/)
This product includes cryptographic software written by
Eric Young (eay@cryptsoft.com)
==========================================================

Input File is input_files/gen_fusescr/ls2088_1088/input_fuse_file
/flexbuild/packages/firmware
building dependent /flexbuild/build/firmware/u-boot/ls1021atwr/uboot_ls1021atwr_tfa.bin ...
Please add the dependent /flexbuild/packages/firmware/u-boot/configs/ls1021atwr_tfa_defconfig
make[1]: Leaving directory '/flexbuild/packages/firmware'
make: Leaving directory '/flexbuild'




Inside of the directory: /flexbuild/packages/firmware/u-boot/configs/, I see the following *_tfa_defconfig files:

 

 

please advise

Outcomes