AnsweredAssumed Answered

Questions about Code Warrior RCW Override (using T1042)

Question asked by Yusuf Altıparmak on Jun 24, 2020
Latest reply on Jun 29, 2020 by Yusuf Altıparmak

Hello Community,

 

I have few questions about Code Warrior PA RCW Override Method.

 

1-) When I select Target Type as "T1042", does it means Code Warrior Tab is not going to bring up the board with the RCW values on it's given flash location (In t1042, for current bank, its 0xE800_0000). Does this mean, If it finds a valid rcw in this flash location, it will read it and bring the board up ?

 

 

2-) If it's chosen with some custom RCW override values, will it ignore RCW on the flash and bring the board up with given values on override .txt file ?

 

 

3-) If my custom board has a valid RCW in 0xE800_0000 and if I choose normal "T1042" option in Target Type section, should it bring up in normal conditions ?

 

Regards.

Outcomes