AnsweredAssumed Answered

The demo "enet_rmii_udp" project cannot work

Question asked by yuan mengmeng on Jun 23, 2020
Latest reply on Jun 24, 2020 by Petr Stancik

Hi,

        During debug the ethernet_udp software,I find a very strange problem. To the ENET_UDP_Tx(testData, 10) function,  when the  data length is set to 10, then the  interface works normal , I can use the Wireshark capture the data. While the data length is set to 20, ENET_UDP_Tx(testData, 20) , then the function become unnormal , the Wireshark cannot capture the transmitted data, only can capture some broadcast frame, of course the PC can success ping to the board.

       I don't the reason why. Can you give me some suggestion? The project as below.

Thanks.

Attachments

Outcomes