KMZ60 Magnetic Sensor, What field strength is needed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KMZ60 Magnetic Sensor, What field strength is needed?

978 Views
fragg
Contributor I

Hello,

for my Project I use the KMZ60 Magnetic Sensor.

From the Datasheet I can read out, that a external magnetic field strength of minimum 25 kA/m is needed for measurement.

But it's not described where I need the 25 kA/m on the chip exactly. Maybe 1mm above the Chip or 2mm, 3mm ....

Or is this value just given, so that they can guarantee their specifications of the datasheet ?

pastedImage_1.png

Kind regards

Florian Ragg

Tags (1)
0 Kudos
1 Reply

933 Views
wtfan
NXP Employee
NXP Employee

Hi Florian,

The 25kA/m is the requirement at reading point as marked in the Fig16 and Fig 17 of datasheet(Fig 17 indicated the extra airgap inside package), this requirement is to ensure the specification of angle error. 

For KMZ60 NXP is planning a PCN soon, your Disti partner should have received a advanced PCN already from NXP, in case you are planning some project qualification,  I suggest that you contact your Disti partner or responsible NXP sales to request for samples with PCN implemented (available from Aug.2020 onwards).

Hope that is clear.

Regards,

Wenting

0 Kudos