AnsweredAssumed Answered

The program I used is the example project with the name of  wdg_pal_interrupt_mpc5744p. When I try to build the project, the type bool can not be resolved. close the project and re-open it ,the error will disappear. 

Question asked by 建永 王 on Jun 19, 2020

The program I used is the example project with the name of  wdg_pal_interrupt_mpc5744p. When I try to build the project, the type bool can not be resolved. close the project and re-open it ,the error will disappear.  when open the file fccu_driver.c ,the bool err will appear again ,I have no idea to solve this issue.....And how to solve it ?

Outcomes