Starting pointers for i.MXRT1060 connected to FPGA using FlexSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Starting pointers for i.MXRT1060 connected to FPGA using FlexSPI

848 Views
palak_shah1
Contributor II

Hi,

We are using IMXRT1060 and using Flex SPI to connect it to FPGA. Both Port A and B are connected to FPGA, so we will be using 8-bit bus. 

Can you please suggest me some starting pointers that can help me understand what to implement? I am looking at evkmimxrt1064_flexspi_nor_polling_transfer

Is this the closest example that I can look at? 

Thanks,

Palak

Tags (1)
0 Kudos
1 Reply

801 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Palak, 

Yes, this is the closest example project that we have. Unfortunately, we don't have an example project that demonstrates how to interface an FPGA with an RT. 

Just as heads-up, the RT1060 family has two FlexSPI interfaces. It's important that you connect your external memory to one fo these interfaces and the FPGA to the other one. 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

0 Kudos