AnsweredAssumed Answered

MIMXRT685-EVK

Question asked by Ray Deng on Jun 15, 2020
Latest reply on Jun 29, 2020 by Victor Jimenez

Dears,

 

I use NXP LPCScrypt to program MIMXRT685-EVK to JLINK debug probe, but it runs error, and cannot change to JLINK probe. CMSIS-DAP is OK to program. You can check the below log and advice.

 

 

////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

LPCScrypt - J-Link firmware programming script v2.1.1 Jan 2020.

Connect an LPC-Link2 or LPCXpresso V2/V3 Board via USB then press Space.

请按任意键继续. . .

Booting LPCScrypt target with "LPCScrypt_228.bin.hdr"
LPCScrypt target booted
.
Programming LPCXpresso V2/V3 with "Firmware_JLink_LPCXpressoV2_20190404.bin"
Error: <Command line>:1: Verify Error 0xb 0x1a0000e0
Script cmd: program E:\ProgramFiles\LPCScrypt_2.1.1_15\probe_firmware\LPCXpressoV2\Firmware_JLink_LPCXpressoV2_20190404.bin BANKA
Last target cmd: =programPage 1a000000 8
Terminated with errors
ECHO is off.
Retrying ...
Error: <Command line>:1: Verify Error 0xb 0x1a000000
Script cmd: program E:\ProgramFiles\LPCScrypt_2.1.1_15\probe_firmware\LPCXpressoV2\Firmware_JLink_LPCXpressoV2_20190404.bin BANKA
Last target cmd: =programPage 1a000000 8
Terminated with errors
ECHO is off.
Retrying ...
Slowing clock ...
..
Programmed 65476 bytes to 0x1a000000 in 1.056s (60.559KB/sec)

LPCXpresso V2/V3 programmed successfully:
- To use: remove DFU link and reboot.

Connect Next Board then press Space (or CTRL-C to Quit)

Press any key to continue. . .


Programming LPCXpresso V2/V3 with "Firmware_JLink_LPCXpressoV2_20190404.bin"

 

 LPCXpresso V2/V3 programmed successfully:
- To use: remove DFU link and reboot.

 

Connect Next Board then press Space (or CTRL-C to Quit)

 

Press any key to continue. . .

 

Thanks & BRs,

Ray

Outcomes