Looking through the NHS3100 SDK v12.3 BETA, there seems to be C# Xamarin cross-platform source code and native platform source code.
Do these code bases have the same features or are there significant differences? Does one code base have more bugs than the other?
Hi,
Well, it's software, so both are likely to have bugs. IMO, the apps from XF folder seem to be more intuitive and easier to use.
Btw, the current iOS and Android listings in the Play/App store are built using the XF code from the internal development branch.
BR,
Dries.