AnsweredAssumed Answered

Manage WiFi Connectivity from C code

Question asked by Nissim Beja on Jun 9, 2020
Latest reply on Jun 9, 2020 by gusarambula

Hi,

 

I am developing a tiny IoT device which is based on the i.MX8 nano.

Currently i am using the NXP evaluation kit that supports the i.MX8 nano.

My goal is to build a tiny embedded Linux distribution with Yocto that provides

A console only image that fully supports the target device hardware (NO X11 \ XWayland)

I would like to hear suggestion \ recommendation how can i manage the WiFi connectivity from c code by using APIs. 

Managing the WiFi connectivity tasks could be:

Switching from WiFi hot-spot to WiFi client mode, get notification about connection \ disconnection events and so on.

 

Is it possible to use Network Manager?

 

Regrads,

Nissim

Outcomes