AnsweredAssumed Answered

T2080 Reference Board

Question asked by Hemant Kumar Tiwari on Jun 3, 2020
Latest reply on Jun 5, 2020 by Hemant Kumar Tiwari

Hello,

Currently i am working on the device is based t2080 processor. 

In the design i am only using one Ethernet phy i.e. RTL8211E-VB.

As i am not using 10G EDC PHY CS4315, can i connect the SD1_REFCLK2 and SD1_REFCLK2 to U47 ICS843002-01? If yes, then why it is not connected in the reference design?

 

To understand better, i am enclosing the image for the same.

 

Waiting for your reply,

 

Regards

Hemant

Attachments

Outcomes