2GB Micron DDR4 configuration for i.MX8M Nano

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2GB Micron DDR4 configuration for i.MX8M Nano

2,105 Views
oferausterlitz
Senior Contributor II

Hello,

We're trying to generate DDR configuration for our i.MX8M Nano board with 2GB Micron DDR4 DRAM. The DRAM datasheet is available at https://www.micron.com/products/dram/ddr4-sdram/part-catalog/mt40a1g16knr-075 

Attached you can find our PRA Tool configuration. The problem is that DDR Stress test tool V3.10 fails to properly recognize DRAM size (1GB instead of 2GB): The output of the tools is :

*************************************************************************
       MX8 DDR Stress Test V3.10
       Built on Feb  5 2020 13:02:45
*************************************************************************

--Set up the MMU and enable I and D cache--
   - This is the Cortex-A53 core
  - Check if I cache is enabled
  - Enabling I cache since it was disabled
  - Push base address of TTB to TTBR0_EL3
  - Config TCR_EL3
  - Config MAIR_EL3
  - Enable MMU
  - Data Cache has been enabled
  - Check system memory register, only for debug

   - VMCR Check:
   - ttbr0_el3: 0x97d000
   - tcr_el3: 0x2051c
   - mair_el3: 0x774400
   - sctlr_el3: 0xc01815
   - id_aa64mmfr0_el1: 0x1122

  - MMU and cache setup complete

*************************************************************************
            ARM clock(CA53) rate: 1500MHz
            DDR Clock: 1200MHz

============================================
        DDR configuration
DDR type is DDR4
Data width: 16, bank num: 8
For DDR4, bank num is the total of 2 bank groups and 4 banks per group
Row size: 16, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select:   1024MB
Density per controller is: 1024MB
Total density detected on the board is: 1024MB
============================================

I'd appreciate the review of our configuration.

Thanks a lot.

0 Kudos
5 Replies

1,955 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ofer

seems "Number of BANK GROUP addresses" should be 2 per datasheet:

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,955 Views
oferausterlitz
Senior Contributor II

Hi Igor,

Thanks for a prompt reply. The "Number of BANK GROUP addresses" is calculated automatically by RPA tool. Are you saying that this calculation is incorrect and RPA tool should be modified ?

0 Kudos

1,955 Views
oliver_chen
NXP Employee
NXP Employee

Hi oferausterlitz‌,

Yes, you should both change Number of BANK GROUP addresses2 and DDR4 Density per Device (Gb)2 in the RPA.

The tool did not cover all BANK GROUP sistuations.

B.R

Oliver

0 Kudos

1,955 Views
oferausterlitz
Senior Contributor II

Hi Oliver, Igor

Thanks a lot, the modified RPA fixes the problem. Appreciate your help.

0 Kudos

1,955 Views
igorpadykov
NXP Employee
NXP Employee

one can try to set DDR4 Data Bus width per device=8

Best regards
igor

0 Kudos