flexbuild_lsdk1909 build for imx6qsabresd : Missing arch/arm/configs/imx_v7_defconfig and other errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flexbuild_lsdk1909 build for imx6qsabresd : Missing arch/arm/configs/imx_v7_defconfig and other errors

567 Views
madhusudankumar
Contributor II

Was working on lsdk 19.09 for imx6qsabresd . 

When using [root@fbubuntu flexbuild_lsdk1909_update_221019]$ flex-builder -m imx6qsabresd 

got an error while the build was at

"Building the dependent build/linux/kernel/arm32/IMX/uImage ... "

Error
*** Can't find default configuration "arch/arm/configs/imx_v7_defconfig"! 

So copied one of the defconfigs named "imx_v6_v7_defconfig" to "imx_v7_defconfig" 

Again started the build ,but now getting the following error 

build/firmware/u-boot/imx6qsabresd/imx6qsabresd_boot.scr [Done]
INSTRUCTION: mkbootpartition
DESTARCH: arm32
PORTFOLIO: IMX
CONFIGLIST: build_lsdk.cfg
INSTRUCTION: mklinux
DISTRO TYPE: yocto
DISTRO SCALE: tiny
DESTARCH: arm32
PORTFOLIO: IMX
CONFIGLIST: build_lsdk.cfg
FATAL ERROR: Couldn't open "../../build/linux/kernel/arm32/IMX/imx7ulp-evk.dtb": No such file or directory

Unable to Proceed further

#layerscape#lsdk

Tags (2)
0 Kudos
1 Reply

512 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Madhusudan Kumar R,

I have moved this thread to the layerscape community. They may be able to provide better guidance on how to port the lsdk to the i.MX, if possible, as they are more familiar with this sdk.

My apologies for the inconvenience.

Regards,

0 Kudos